DYNXAMIXEL model: 2XL430-W250
Phenomenon: There is a zero deviation problem on one axis of the dual axis servo. Is there any calibration operation. Here are a few photos:
1.The zero position of the steering gear is now not aligned with the marking line of the zero position of the steering gear.
2.Using the self diagnosis function in the dynamic wizard,
The actual situation does not match the figure.
3.Select the calibration function of the upper computer, which is not available. I’m not sure if it is not supported.
4.The zero position of the other axis is normal: