There aren’t any available tutorials specifically on modifying the existing OpenMANIPULATOR-X to add an additional joint, as far as I am aware.
Your assumption about a 6DOF OpenMANIPULATOR are correct though, all you would need to do is add an extra XM430-W350-T and some frame pieces to mount it. Although, one important consideration is that adding an additional joint near the manipulation end of the arm will reduce the maximum payload capacity.
You’ll need at least two frames in order to add the extra actuator. One to attach the casing to the previous joint, and one to attach to the horn to the next actuator. The specific frames that you’ll need also depend on the way you want to attach your additional joint.
The plastic linkages are unfortunately not available for sale separately, but the 3D printable files of those as well as all of the other plastic components are available to fabricate your own.
Hey, just wanted to know if you were able to make it a 6DOF system or not. We have the same challenge. We have already connected the new dynamixel to the arm and we are able to control it using dynamixel wizard. Now we want to define the new dynamixel (joint) and frame (link) in the software so it can be controlled using MoveIt and be considered as a part of the arm chain. We would appreciate if you would help.