Chi,
I think I figured out the problem - here is the result of a “conversation” I had with ChatGPT regarding the data flow in and out of the Arduino USB port:
##### You said:
what does /dev/ttyUSB0 refer to when configuring a serial port on a RPi USB port
###### ChatGPT said:
ChatGPT
On a Raspberry Pi, /dev/ttyUSB0 is a device file that represents a USB-to-serial adapter connected to a USB port on the Pi. When configuring a serial port through USB on a Linux system, these device files (/dev/ttyUSB0, /dev/ttyUSB1, etc.) are automatically created by the OS each time a USB-to-serial adapter is connected.
Here’s a breakdown of what each part means:
** /dev/: This is the directory where device files are stored on Linux systems.*
** ttyUSB0: This specific file name is for a USB-based serial interface. The number (0) indicates it’s the first USB serial device detected. Additional adapters would show up as ttyUSB1, ttyUSB2, and so on.*
When configuring a serial port to communicate with an external device (e.g., a microcontroller or sensor) over USB, you’ll typically use this device file to establish communication. It allows you to set parameters like baud rate and transfer data to and from the external device over the serial connection.
##### You said:
so /dev/ttyUSB0 makes a USB port emulate a UART?
###### ChatGPT said:
Yes, exactly! The /dev/ttyUSB0 file allows the USB port to emulate a UART (Universal Asynchronous Receiver-Transmitter) serial interface. This setup uses a USB-to-serial adapter (typically a chip like the FTDI, CP2102, or CH340) to convert USB signals into standard UART serial communication.
Here’s how it works:
1. USB-to-Serial Adapter: The adapter (or chip) bridges the USB and UART protocols. It handles the conversion of data between USB signals and the TX/RX (transmit/receive) lines used in UART communication.
2. Device File /dev/ttyUSB0: When you plug in a USB-to-serial adapter, the Linux kernel detects the device and creates a device file like /dev/ttyUSB0. Programs can then open and use this file to send and receive serial data just as they would with a native UART port.
3. Communication: With this setup, you can use standard serial communication parameters (like baud rate, data bits, stop bits, and parity) over the USB port, allowing you to interact with UART devices such as microcontrollers, GPS modules, or sensors that communicate over a UART interface.
In short, the USB-to-serial adapter and /dev/ttyUSB0 together make it possible to connect and communicate with traditional UART-based devices through a USB port.
##### You said:
is the USB connector on an Arduino NANO a USB port or a UART
###### ChatGPT said:
The USB connector on an Arduino Nano is technically a USB port, but it is used to emulate a UART (serial) interface. This is achieved through a USB-to-serial converter chip on the Nano.
Here’s how it works in more detail:
1. USB Port on the Nano: The Nano’s USB connector (usually a mini-USB or micro-USB) physically connects the board to a computer over USB.
2. USB-to-Serial Converter Chip: Older Arduino Nano models typically have an FTDI FT232 chip, while newer versions might use a CH340 or CP2102 chip. This chip acts as a USB-to-UART bridge, converting USB data from your computer to UART signals that the Arduino’s microcontroller (e.g., ATmega328) can understand.
3. Emulated UART Communication: The computer communicates with the Arduino Nano over a virtual serial port (such as /dev/ttyUSB0 on Linux or COM3 on Windows), which mimics a traditional UART interface. Data sent through this virtual serial port is converted by the USB-to-serial chip and received as UART data by the microcontroller.
4. Serial Monitor & Programming: This emulated UART connection allows you to both program the Arduino (upload code) and communicate with it through the Serial Monitor in the Arduino IDE, as if it had a native UART port.
So, while the physical connection is USB, the interface emulates a UART through the use of the USB-to-serial converter, making it appear as a standard serial port for most purposes.
##### You said:
so when I send data out of an Arduino USB port, it is actually a UART communication
###### ChatGPT said:
Yes, when you send data from the Arduino Nano’s USB port, it is actually UART communication being transmitted over USB. Here’s what happens:
1. USB-to-UART Conversion: Data you send over Serial (like Serial.print() in Arduino code) is handled by the USB-to-serial converter chip on the Nano (like the FTDI or CH340). This chip converts the UART data into USB protocol packets so that it can travel over the USB cable.
2. Virtual Serial Port on the Computer: On the computer side, these USB packets are received by the operating system, which translates them into data accessible through a virtual serial port (e.g., /dev/ttyUSB0 or COM3). This virtual serial port lets your computer interact with the Arduino as if it were connected via a traditional UART interface.
3. Emulated UART Communication: From your code’s perspective, the data is being sent and received over a UART serial interface, but it is encapsulated in USB packets for transport over the USB cable.
So, while the physical connection is USB, the communication itself emulates UART. This is why you can use typical serial communication functions and settings (like baud rate) despite using a USB cable.
In summary:
** On the Arduino side: UART data is generated by the microcontroller.*
** In transit: The USB-to-serial chip converts UART data to USB packets for transport.*
** On the computer side: The USB packets are reinterpreted as UART data by the OS, making it accessible as a standard serial port.*
So, conceptually, yes—the data you send from the Arduino Nano’s USB port is UART communication at its core, sent over USB. [Frank: key point]
So, Chi, I think as per your suggestion, the answer is to use the other serial UART on the Arduino, TX1/RX1, rather than trying to use the USB port…
I guess a good clue there is that I can always still connect the Arduino to the PC via the Arduino USB port when I am programming, but cannot do the same with the RPi’s USB port that I use to connect to the CM-530 unless I force it into “device” mode…
So, I have a bit of work to do here but I think I have a plan - I’ll keep you posted!
Frank