Hi All, This is the ROBOTIS Technical Support Team,
I would like to share how the Byte Stuffing work in DYNAMIXEL with very simple example.
According to the explanation on Byte Stuffing in e-Manual, it says
Processing Order of Transmission
- Generate basic form of Packet and afterwards Byte Stuffing(0xFD)
- Inspection range : Everything within the Instruction field to the Parameter field (not the CRC)
- Processing method : When the pattern “0xFF 0xFF 0xFD” appears, add Byte Stuffing (0xFD) (If “0xFF 0xFF 0xFD” already exists, add a 0xFD to change it to “0xFF 0xFF 0xFD 0xFD”)
Here is the brief example I did for you to understand the DYNAMIXEL Byte Stuffing.
- To produce the example simply, I linked Goal Position (Extended Position Control Mode(Multi-turn)) and Goal Current by Indirect Address
-
The rule of constructing packet is Littile Endian, which put the LSB first and MSB if simply describing. The address 224 to 229 reference the corresponding address of Indirect Address.
-
Let’s send 0XFF | 0XFF | 0XFF | 0XFF | 0XFD | 0X01and see how the packet structure is actually constructed.
- As e-Manual described, you can see
FDis actually stuffed between “Header” look-like packets in order to avoid embarrassing situation by the hader look-like !
Thanks,