Can I use BT-410 and dongle to re-firmware the CM-530 controller, and use it to import the hex file into the controller?

Use the following template to help create your post:

  1. What model of servo are you using?
    AX-12A and AX-18A

  2. Describe your control environment. This includes the controller or interface, and any power source.
    CM-530, R+ manager, R+ terminal, Embedded CM-530, Eclipse

  3. Specify the operating mode for applicable models, and any firmware settings you are using.

  4. Include pictures if possible.

  5. Include a full description of the issue.
    I have broken the mini usb port of CM-530 controller. Now I want to import the hex file into it. Can the BT-410 module and it dongle can help me to import the hex file form computer into the controller? Or do I have the other way to make it? Please help me.

In the past, I was able to recover the ROBOTIS Firmware on a CM-530 using the LN-101 and Manager 1. However, I had never tried to import my own hex file to the CM-530 using the LN-101.

1 Like