Issue:
This is our first time building a Level 3 robot from the Robotis Dream II Level 3 kit. I downloaded the R+Task 3.0 App to my MacBook Air. We can’t seem to get the CM-150 to connect. I click on the option to use USB Dongle and what I believe to be that automatic search function. It’ll switch from the Searching to Connecting message but then won’t move past that.
It sounds like maybe something with the drivers from my searching but since I’m on a Mac I don’t know how to double check all that. Thank you for any help!
On the CM-150 itself did you have the BT-410 module hooked up to it?
If you did, it should have paired automatically to the USB BT-410 Dongle (both LEDs should become solid blue)?
However there is a trick for First-Time use. You have to get the USB dongle real close to the BT-410 on the CM-150, about 1 inch. Then they should pair automatically. From then on they can be farther apart and still pair to each other properly.
Check your drivers. Also, are you sure the controller is opened?
I don’t believe we have the BT-410?
This is where I need the help for sure. How do I check that we have the appropriate drivers? And how do we know if the controller is open or not? Forgive my ignorance, brand new to all of this.
Well, good news! We got the program downloaded but had to use R+2 to connect. R+Task3.0 wouldn’t connect.
Congratulations! Well done. If you can run Task 2 you must have some kind of Windows Emulation software?
If so try to use the Robotis Manager 2 tool also so that you can update the CM-150 firmware via the USB cable.
1 Like