Use the following template to help create your post:
-
What model(s) of servo are you using?
XM430, but can use AX12A as well, if needed -
Describe your control environment. Include the controller or interface, operating system (and version #) of your computer, and how you are powering your robot.
I am using Teensy 3.2 (can use 4.0 if needed) and I’m trying to control a Dynamixel XM430/AX12A motor, and I’m powering the robot using batteries.
I tried several Arduino libraries (mainly “Dynamixel2Arduino” and “Dynamixel”), but the problem is that I cannot use a shield (since I’m using Teensy, and there is no Dynamixel shield for Teensy) so I have problems reading data from the motor. I managed to send data (e.g. write degree, turn led on/off and so on) but couldn’t read any data.
I figured out it has something to do with the TTL communication, and half/full duplex, which the Dynamixel requires in order to work, and unfortunately the Arduino (/Teensy) isn’t able to provide on its own.
I tried to look up online for ways to solve this issue, however I really couldn’t find anything, it seems as if I’m the only person who have this setup - Dynamixel with Teensy. (or any other Arduino board without a shield)
Is there a way I can achieve my goal? Which components do I need?
Any piece of information will be highly appreciated, thanks in advance! ![]()