Contrôle dynamixel AX12A avec Arduino (interfaçé avec Shield)

DYNAMIXEL Actuator

DYNAMIXEL-AX-12A

Issue Description

I can upload the program but it doesn’t run

Additional Information/Attachments

Dynamixel AX-12A_Shield_Arduino

Would you be able to provide some more information about the kind of issues you are experiencing?

  1. What program or example are you trying to run?
  2. Does the red light on the back of the AX12 blink when you connect it to power?
  3. Do you have an LN101 or BT410 that can be used to access the serial monitor output?

Any more information you could provide beyond these questions would also be helpful in allowing me to provide you with assistance.