Use the following template to help create your post:
1.I am using XL330-M077-T, XM430-W350-T, XL430-w250-T.
2.I Use U2D2 with 5v and 12V power source depending on the motor i try to control.
- I am trying to use the two 430 motors of the mentioned list above. I tried dynamixel wizard. i am unable to detect both motors at the same time. The motors are detected and controllable if i connect them separately but not when i connect both motors to the U2D2+Powerhud or U2D2+Exp485 at the same time.
I need support to know if i am doing something obviously wrong.
Thanks in advance.