Hello everyone, im working with 4 Dynamixel XL-320 using an OpenCM 9.04 to control them.
Im using an exernal power source to power up them with 10v.
The problem is that Im trying to upload a firmware recovery on them beacuse the led stopped blinking when power on connected to the OpenCM 9.04. All 4 xl-320 used to work properly but now they are not responding, and while doing the firmware recovery on R+ Manager the program shows me this error: The installation failed, as shown in the picture below.
They used to work correctly, even using the scan dynamixel example in Arduino found them but now the program cant found them.
Also, Im trying to do a firmware recovery one by one.
Is there any solution to this? Thanks in advance.