fayad
February 19, 2024, 2:38pm
1
Hi
I try op3 manager with 2 MX-28, 6 MX-64, 12 XM540-W270
a weeks ago, the servo can work as well. but today, when i try to run the op3manager this massage appear
[ERROR] [1707646848.403888959] Failed to turn on the power of DXLS!
i have changed the power output wire that looks bad, but still didn’t work, what must i do??
Thank you very much
fayad
Do you have a U2D2 that you can use to test them one by one?
fayad
February 26, 2024, 2:51pm
3
i do, but when i try to turn on opencr, the dynamixels pilot Lights up only less than 1 second. does my opencr have the power issue, or just the wiring failure??
When first powered on, the DXLs always flash the LEDs very briefly - this is a good sign that they are working.
Unfortunately, I do not use the OpenCR, so I can’t help much more.
You can always use the OpenCR just to power the DXLs, and then tap one DXL at a time to your U2D2 to check it out with DXL Wizard 2.