How Does current mode work in XM430-W210?

Hello, I’ve been working with Dynamixel’s XM430-W210, I’m trying to use the current mode, but I’m not really sure how it works.
My questions are:

  1. How Does the current mode exactly work?
  2. Is there a Block diagram describing the current mode controller? A diagram as those describing velocity and position mode controllers in the e-manual.

Thank you in advance.

Hi @diegoene17, thanks for your question and for posting on our new page! Sorry for the slight delay in response; I’ve been offline for a bit working on projects. I should be able to share some information to clarify:

The current-based control modes for DYNAMIXEL XM430-W210, and other models of X-series that offer Current Control and Current-based Position Control, can be used for different applications depending on your goals.

Current Control Mode allows the user to specify a direct Goal Current that the DYNAMIXEL will use to turn endlessly in that direction, at the force allowed by the current level. This can be ideal for applications supporting / measuring a load, or for force-limited operation with gear reductions.

Current-Based Position Control Mode allows users to specify both Goal Current and Goal Position for the DYNAMIXEL to move to. While moving to the Goal Position, the DYNAMIXEL will work not to exceed the Goal Current. This can allow for force-limited motions in collaborative robots and other applications.

For block diagrams, unfortunately I do not have a specific diagram for the Current Control Mode, but the Current-Based Position Control mode diagram is listed in the e-Manual for XM430-W210 and I’ll paste it below:

Allow me to check in with @Tech_Support and @Yogurt_Man to see if they might be able to share more information on the current control mode block diagram.

Let me know if you have any other questions!

2 Likes

What up @diegoene17

Make sure to switch Operating Mode (11) to the Current Based Position or Current control Mode.
Honestly, the block diagram should be just used as the reference. You may want to see the Present Current(132), Goal Current(102) and Performance Graph. Generally, #1 a torque is proportional to the provided current to the motor, so that if you can control the providing current to the motor, you can control the torque (In this case, Goal Current is the reference) #2 If you can measure the current in the motor, you can actually sense the force by looking at the current (In this case, the Present Current is the reference)

The performance Graph is showing the conversion values between the current to the torque.

Hope this information helpful,

Good day,