Issue with Updating to TASK V. 3.1.11 on Windows 11

Issue:
@ROBOTISUSA and @Jason

Today, when I opened up my TASK V.3, it asked if I wanted to update to Version 3.1.11. So I went ahead and got it updated. And the update ended with a success message.

But when I started TASK 3 back again it flashed this message real quick

image

And then TASK 3 just shut down. Obviously something to do with the UNITY engine. I am running the latest Windows 11.

Thanks

If you go to the installation path for R+ Task 3.0 and delete “UnityCrashHandler32” it should work properly.

Example installation path: C:\Program Files (x86)\ROBOTIS\RoboPlus 3.0\R+ Task 3.0

Thanks

1 Like

@YKW_R

Thank you very much for the update.

On my Windows11, I only have UnityCrashHandler64.exe.

image

So I deleted UnityCrashHandler64.exe. Then I updated TASK to V.3.1.11. It installed OK again. But it put back UnityCrashHandler64.exe. And the same error condition still happened when I started the updated Version of TASK 3.

So I went back in and erased UnityCrashHandler64.exe once more and now TASK V. 3.1.11 works OK!

This topic was automatically closed 3 days after the last reply. New replies are no longer allowed.