The KINDER user manual offers 16 robots that users can build, but in case users need more robot designs to play with, the following robots can be built using the existing parts of the KINDER kit.
BOXER (derived from the KNIGHT)

THUMB BOXER (derived from an OLLO J kit) using NIR Sensors #5 and #6 to trigger punching from the robot: NIR 6 for the left arm, NIR 5 for the right arm.

BATTLE BOT (derived from HELICOPTER’s concept but actually powered)

WINDMILL (also derived from HELICOPTER’s concept but actually powered)

SEGWAY by duplicating and shifting Motor Axles forward.

4-WHEEL DRIVE by duplicating and shifting twice the Motor Axles forward.