I am using the XM430 - W350 -T Dynamixel motor with the OpenCR board . I currently have no load on the motor and am using the Dynamixel wizard to troubleshoot. I have tried in velocity and position mode to get the motor to work and the motor is in a pattern of running for a second, turning off and sending an overload error, and then not running again at all until I let it sit unplugged for a bit. The motor has no load and its gears are working correctly.
The motor was working perfectly before and now isn’t working at all. Please help