Hi, I am currently using OpenRB150 to control actuators and sensor data reading.
I noticed that either the sensor data reading or the RC100 works well. But when configuring both of them, it always failed.
I realized this is resulted by configuring multiple serial ports in Arduino sketch.
Just wondering in this case, how should I configure both the sensor and RC100 simultaneously?
The code for RC100 setup: Serial.begin(57600); Controller.begin(2);
The code for sensor setup: Serial.begin(115200); Serial.println(“MPRLS Simple Test”); if (! mpr.begin()) { Serial.println(“Failed to communicate with MPRLS sensor, check wiring?”); while (1) { delay(10); } } Serial.println(“Found MPRLS sensor”);
Serial() points to the USB Port on the OpenRB-150, meaning the Serial Monitor tool on your Arduino IDE. And it looks like that first you set Serial() to 57600 bps, then later you change it to 115200 bps >> this is the problem: you need to choose only one baud rate for the Serial Monitor.
Controller.begin(2) means that you are using Serial2 for your RC-100 Controller, this got nothing to do with Serial(). ROBOTIS restricts all their BT-210/410 to 57.6 Kbps.