MX-64 Cartesian Trajectory Planning

Use the following template to help create your post:

  1. State the model of servo you are using.
    3*MX_64

  2. Add (or create) Tags to your post with the specific model of your product.

  3. Describe your control environment. This includes the controller or interface, computer and OS, and any power source you are using
    I am using Labview, Dyanmxiel SDK, protocol 2.0 Labview block.

  • 列表条目

baud rate is 57600

  • 列表条目

image

  1. Specify the operating mode you are using, for applicable models.
    I am using position mode for three MX-64

  2. Specify and link any manuals or resources you have used related to your inquiry.

  3. Include pictures if possible. This can help our members see how wires are connected, how hardware is installed, or to identify other possible issues.
    9125d011bc3c51b0a51ed605e8bc064
    My target is make a endpoint of my robot move following straight line, not arbitrary movement.
    I designed a Cartesian space trajectory planning and
    step1: create the points(array) with inverse algorithm-> joint Pos (array)
    step2: release joint pos every 50ms to Mx-64
    But in the real experiment, when robot move, there are very big joggle in each motor.
    On the another hand, without Cartesian trajectory planning,
    I just control each joint by position mode,
    there are smooth.

so what is the potential problem with this, I believe you have some application which is operating in Cartesian space, could you give me some advice.
thanks a lot!!

9125d011bc3c51b0a51ed605e8bc064