Issue:
I using openRB-150 to control 18 DOF hummanoid (all ax-12)
It work pretty well, but sometimes suddenly all actuator stop work.
To recover this situation, I have to disconnect all four dynamixel cable to Open RB-150 and re-connect.
I heared that Open RB 150 support maximum 14 dynamixel ( I don’t know where i get this info)
Is this situation  occured from this reason?
I give openrb external power source 12V5A (robotis SMPS 12V 5A PS-10)
PROVIDE A THOUROUGH DESCRIPTION OF YOUR ISSUE, THE MORE DETAIL YOU PROVIDE THE EASIER IT WILL BE FOR THE COMMUNITY TO PROVIDE YOU ASSISTANCE
DYNAMIXEL Servo: AX-12
LIST ALL DYNAMIXEL SERVOS USED IN THIS PROJECT
DYNAMIXEL Controller:Open RB-150
LIST ALL DYNAMIXEL CONTROLLERS USED IN THIS PROJECT
Software Interface:Arduino IDE
LIST ALL SOFTWARE INTERFACES USED IN THIS PROJECT