Open RB-150 shows as unknown usb device

Issue:
after doing python-arduino serial communication scatch,
suddenly my pc cant detect open-rb
and i got code 43 error
https://answers.microsoft.com/ko-kr/windows/forum/all/usb-장치-인식/7682a29b-8e1c-4c49-980c-b293a74b801b

how ever i can detect device in bootloader mod.
what can i do now?


DYNAMIXEL Servo:

LIST ALL DYNAMIXEL SERVOS USED IN THIS PROJECT


DYNAMIXEL Controller:

LIST ALL DYNAMIXEL CONTROLLERS USED IN THIS PROJECT


Software Interface:

LIST ALL SOFTWARE INTERFACES USED IN THIS PROJECT

Have you tried reuploading the Arduino sketch while the OpenRB is in bootloader mode?

This happened to me as well. I was successfully uploading sketches and controlling dynamixels, when all of a sudden - It froze in ‘uploading…’. then the USB disconnected, and I got the unknown USB device error (43). Hitting reset button on IMU shield got back USB connection, however, uploading a sketch still hangs. The suggestion above about uploading in bootload mode worked! So, instead of uploading at COM6, I upload at COM8.