Use the following template to help create your post:
-
What model of servo are you using?
OpenCR board -
Describe your control environment. This includes the controller or interface, and any power source.
CPU: Raspberry pi4
Controller: OpenCR
Powersource: PC, given battery, given charger -
Specify the operating mode for applicable models, and any firmware settings you are using.
Default as per e-manual steps -
Include a full description of the issue:
Hi everyone,
I am currently having some issues with my OPENCR board, and I was hoping to get some help troubleshooting the problem. I am using a Raspberry Pi 4 connected to the OPENCR board via the Raspberry Pi’s USB port. Here are the symptoms of the issue:
- The OPENCR board does not appear to be booting up properly. The status light on the board is always off unless I reset it, in which case it seems to work okay.
- When I try to upload code through the Arduino IDE, I get an error stating that the port could not be found.
- I have tried reinstalling the firmware by resetting the board and uploading test scripts via the Arduino IDE. I have also tried reinstalling the software multiple times using the Raspberry Pi.
- On the bringup step, I get an error when running “ros2 launch turtlebot3_bringup robot.launch.py” stating that “ld08_driver” is not found, even though it is in the home directory.
Based on these symptoms, I suspect that there may be a firmware problem with the OPENCR board, but I haven’t been able to successfully reinstall it. Can anyone offer any suggestions for how to troubleshoot this issue and get my OPENCR board working properly?