Issue: OpenRB-150 not detecting XL330-M288-T
PROVIDE A THOUROUGH DESCRIPTION OF YOUR ISSUE, THE MORE DETAIL YOU PROVIDE THE EASIER IT WILL BE FOR THE COMMUNITY TO PROVIDE YOU ASSISTANCE
I have wired this board using terminal VIN and with an external battery and my computer detects the board on COM6 as (Arduino MKR Zero).
But when I plug the XL330-M288-T servos into the board, no lights turn on for the servos at all. I have tried plugging into all of the ports and scanning for the servos in the Dynamixel wizard 2.0 but the program is not able to detect the servos at all when I try to scan.
I have tried running the position_mode example in the arduino IDE. The program is able to upload to the board but nothing happens with the servos.
Thank you in advance for your assistance.
DYNAMIXEL Servo: XL330-M288-T
LIST ALL DYNAMIXEL SERVOS USED IN THIS PROJECT
DYNAMIXEL Controller: OpenRB-150
LIST ALL DYNAMIXEL CONTROLLERS USED IN THIS PROJECT
Software Interface:
LIST ALL SOFTWARE INTERFACES USED IN THIS PROJECT
Arduino IDE, DYNAMIXEL Wizard 2.0