Hello, I hope you can help me. I am working on a project with Bioloid Premium robots (humanoid type C and king spider). But I ran into software limitations, especially 3.
1. The humanoid does connect to my computer with the RoboPlus and R+ Motion 2.0 programs, but with programs like R+ Task 2.0 or newer software, it does not detect the CM-510. So I’ve been working with those two programs without issues, but when I record the default program, the following errors appear in the console:
{[ERROR:8100:0007:02]}
{[ERROR:8100:0008:02]}
{[ERROR:8100:0007:02]}
{[ERROR:8100:0008:02]}
{[ERROR:8100:0007:02]}
{[ERROR:8100:0008:02]}
{[ERROR:8100:0007:02]}
I read the manual and found that:
8100 → is the error ID
0007 or 0008 → is the servo motor ID, but there is no information on 02. I would like to ask for your help to verify what type of error this is.
2. When trying to use the physical remote control, the robot does not respond, do you think the receiver might be damaged?
3. When trying to use the spider king controller (CM-5), no program detects it at all.