I am not sure if this is the right place to post this, but I wanted to have some areas of the dynamixels clarified before I buy them. From looking at the pictures, it seems like there is a main output shaft on the front of the dynamixel and a secondary one on the back. Does the one on the back turn, or is it just a circular mounting pattern?
I was also wondering if it would be possible to independently control dynamixels using the TTL protocol when they are daisy chained, and where I can find the documentation for how a wiring setup with daisy chaining would work. I am planning to use the U2D2 Board and power distribution hub connected to an arduino running ROS 2.