조이스틱(rc-100b)과 젯슨 나노 호환 관련

@harry
I have no direct experience for your situation/need, but I do know about some pieces of the “puzzle” you are trying to put together:

  • Jetson Nano won’t recognize your BT-410 directly, but it may recognize the BT-410 USB Dongle as a “ttyUSBx” Port. BT-410 Dongle - ROBOTIS

  • Then you need to put a BT-410 Slave Module on the RC100-B. At this point your BT-410 Slave will automatically synch to the BT-410 USB Dongle on the Nano (hardware-wise only).

  • Next, you’ll need to interface the ZigBee SDK to your Nano - assuming you are programming your Nano in C/C++
    ZIGBEE SDk
    because the RC-100 uses a particular communication packet with the following format
    RC-100A/100B
    I have done this part before using an LN-101 (wired connection to Jetson Nano and a CM-550), so I know that this part worked OK.