Is Dynamixel wizard 2.0 only supported in Ubuntu 16.04 and 18.04? This seems very outdated. I am using Ubuntu 22.04 with ROS2 humble. I tried installing it anyway and it says:
‘No apps installed that can open “DynamixelWizard2Setup_x64”. You can find more applications in Software.’
Actually, I think it works on Ubuntu 22.04, at least it installed properly.
But the docs were confusing. After I downloaded the file, I thought I just have to run it, which doesnt work. On the docs below, there are full installation guides. It would be less confusing, if the software download was in the corresponding OS installation guide.