Wizard2.0 unable to detect MX64 connected to OpenCM 9.04 + 468 Exp

Use the following template to help create your post:

  1. What model of servo are you using?
    MX64

  2. Describe your control environment. This includes the controller or interface, and any power source.
    OpenCM 9.04 C + 485 Exp with 12v, 5amp power

  3. Specify the operating mode for applicable models, and any firmware settings you are using.
    Open CM 9.04 firmware v25, Dynamixel channel is set to 1

  4. Include pictures if possible.

  5. Include a full description of the issue.
    MX64 is on Protocol 2.0 and detectable using U2D2 but not through OpenCM 9.04 using Wizard2.0. I would like to use OpenCM9.04 to control the servo as well as using Task 3.0 to program poses and motions.

If you plan to use TASK V.3 with the OpenCM-904 + 485-EXP, i.e. using the default ROBOTIS firmware on the OpenCM-904, you’ll have to use MANAGER 2 to access your Dynamixels.