Just to add another datapoint, I bought a single replacement XC330-T288 to replace “102” while the warranty issue is sorted, in exactly the same position on the arm with all the same ventilation it’s sitting at 29c after 15 minutes. The other T288’s still warm up to previous amounts, the servo in the mirror position on the other arm (110) is sitting at 57c.
[16:51:41] : {100: 42, 101: 44, 102: 24, 103: 40, 104: 17, 105: 16, 106: 16, 107: 17, 108: 43, 109: 47, 110: 46, 111: 41, 112: 16, 113: 16, 114: 16, 115: 16}
[17:7:4] : {100: 49, 101: 54, 102: 29, 103: 48, 104: 18, 105: 18, 106: 18, 107: 19, 108: 51, 109: 59, 110: 57, 111: 49, 112: 18, 113: 18, 114: 18, 115: 18}
I’ve no idea what is wrong with these other servos, there’s certainly something not right though.