Use the following template to help create your post:
-
XL-320 servomotor
-
I am using the OpenCM 9.04 board with the OpenCM 485 EXP and a power supply of 12V connected to the OpenCM 9.04.
Issue:
By connecting the XL-320 to the OpenCM 9.04 and powered by the EXP 485 (thanks to a power supply of 12V), the XL-320 does not blink at all and the R+ Manager Firmware Recovery does not find it. I think it is the output voltage on the socket pin for the XL-320 on the OpenCM board that does not have enough output voltage (I measure only 4.8 V) while the specification of the XL-320 indicates that it should be powered for a minimum of 6V…
How can I avoid a battery to power up and use the XL-320 with the OpenCM board please ?
I am struggling here…
Many thanks !