Cm-530과 bt-410 안드로이드 통신

CM-530을 사용 중이고 블루투스를 통해 안드로이드에 통신시키고 싶습니다.

BT-410을 사용해야 할 것으로 보이는데 사용하면 안드로이드와 통신이 가능한지, 어떻게 해야 통신이 되는지를 알고 싶습니다.

@Soft

Back in 2017, I was successful in using the OLLOBOT SDK between an Android phone (using Android Studio) and CM-50, CM-150, and OpenCM-904. But I did not try it with a CM-530, because the CM-530 can only deal with DXL Packet Protocol 1, and the OLLOBOT SDK only deals with DXL Packet Protocol 2. So, you’ll need to make a decision about keeping using CM-530 for your Android project.

Please see these YouTube links for the videos involved - you’ll have to watch them straight from YouTube.

There is a GITHUB for the OLLOBOT SDK at

ROBOTIS also has several special applications (APK files) using the OLLOBOT SDK at this link

https://en.robotis.com/service/downloadpage.php?ca_id=20

There is an OLLOBOT SDK tutorial at

If you are affiliated with a university, you may be able to use the university’s library via Springer-Link to have a look at Chapter 12 of this book with free access.

https://www.amazon.com/Exploring-Robotics-ROBOTIS-Systems-Thai/dp/3319598309

This Springer Extras link has all the example codes for my 2017 book:

There should be several ZIP files with the name “OLLOBOT….zip” for the Android Studio files that were used back in 2017.

It has been a very long time ago, so I am not that conversant with Android Studio anymore, so this is the extent of my knowledge for this topic. :confused:.

Good Luck with your project.

P.S. Back in 2017, the CM-550 did not exist! So you want to take on the challenge to be the first user to interface the OLLOBOT SDK with the CM-550? :smiley: