I need to control the torque of the XM servo motor. Is the current mode ineffective? Is the feedback current accurate
The XM series circuit has a built-in current sensor, which can check the current supplied to the motor in units of 2.69mA.
If controlled in current mode, the torque can be adjusted.