Amala
February 3, 2023, 9:49am
#1
Hi everyone,
DYNAMIXEL System
XM430-W350T
Hardware Description
XM 430-W350t and Pixhawk 6 C.
Robotis Servos — Copter documentation
Issue Description
Control of Dynamixel using ardupilot is still available in ArduCopter V4.2.3 or above?
Robotis Servos — Copter documentation
Thanks in advance
Amala,
DYNAMIXEL control is available on all ArduCopteer versions higher than 4.0
Amala
February 7, 2023, 11:45am
#3
Thank you !
If the Servox_function is diabled, does it work? or do I need to give an actual function,
Is there any way that I can check the connection with the pixhawk?
Unfortunately, I’m not very knowledgeable about the general use of Ardupilot of PixHawk flight controllers.
I would recommend asking over at the ArduPilot Forum to receive some assistance from someone more knowledgeable about this use case.
1 Like