Hello,
I want to know if it’s possible to use XL320’s horn in a XL330 motor.
I did a test and it actually mounts, but when I tried to mount XL330’s horn in the XL320 I noticed that it won’t assembly due to a little difference in the internal (teeth) diameter.
For that, I think that despite XL320’s horn mounts in the XL330 motor, the teeth reliability could be affected. Isn’t it? I’ve measured a difference of 0,3mm in the internal diameter of one an the other.
I need a horn similar to XL320’s in XL330 because I have a project that uses the 4 holes in 320’s horn in order to couple the components. If I have to use XL330 with its horn I should do a heavier adaptation in the project…
Thank you very much for your support!