Use the following template to help create your post:
- What model of servo are you using?
XH540-W270R
I am assembling the horn to the dynamixel by following the video:
[Dynamixel] horn assemble (혼 체결) - YouTube
At 0:48, what does it say? I cannot read the sentence as both the letters and the background are in black. Does it say tighten to push the horn all the way in?
How tight should it be? Even I tightened the screw a lot, there was still an approximately 0.7-1mm gap between the horn and the dynamixel. Is this normal and acceptable? I got several units. Some are like that but others have a much smaller gap between the horn and the dynamixel. When I tightened as much as I could, it was very difficult to rotate the horn by hand even after I had attached a frame to the horn. I had to loosen the screw a bit to be able to turn it.
Will tightening too much damage the motor?