Use the following template to help create your post:
-
What model of servo are you using?
XL430-W250-T -
Describe your control environment. This includes the controller or interface, and any power source.
I am using the OpenRB-150 board powered by a 12V, 5A power source. -
Specify the operating mode for applicable models, and any firmware settings you are using.
I am using the velocity operating mode -
Include pictures if possible.
N/A -
Include a full description of the issue.
I am trying to run the servo at 120rev/min which would correspond to a goal velocity of 524 units. When the velocity reaches about 260 units (~60rev/min) the PWM signal is at its limit of 885 (100%).
Is it possible for the servo to go any faster? My knowledge is quite limited and I’m not sure where to go from here. The present voltage and load were 12V and ~2.4% when I ran into the issue.