Issue: I do not know the maximum value of current that can continue to flow through the Dinamicell XM430-W350-T. I am using a Dinamicell XM430-W350-T. If the motor is over about 1100mA, a “Motor Overload Error” will occur and the motor will stop.
DYNAMIXEL Servo:XM430-W350-T
LIST ALL DYNAMIXEL SERVOS USED IN THIS PROJECT
DYNAMIXEL Controller:
LIST ALL DYNAMIXEL CONTROLLERS USED IN THIS PROJECT
Software Interface:
LIST ALL SOFTWARE INTERFACES USED IN THIS PROJECT