I want motor1 fist move to 512 then when sensor conditions met motor1 move to 850 then move to 180 .Constantly going back and forth from 850 to 180
But I found some problem
1.when sensor condition was met in the first the motor1 didn’t move to 512
2.when sensor condition was me, the motor1only move to 850 didn’t go back to 180
The appropriate solution will depend on the type of actuator used. Is it an older AX or MX actuator? Or is it a newer XL type of actuator?
Also more details are needed. Do you want the actuator to stop at 512 for a short time first? Then flip-flopping between the other two values?
Remember to take into account that any actuator will take “time” to go where your program wants it to go to. Also which controller are you using?
You can also see my YouTube video flip-flopping an AX-12 to understand the various issues involved
안녕하세요.
Goal Position 명령을 주신 다음 해당 목표 지점까지 이동 하는 시간을 줘야 합니다.
Goal Position 이후 딜레이를 추가하여 확인 해주세요.
감사합니다.
thank you help me solve this problem
thank you I had solved this problem
You are welcome, but I can see that you prefer short answers over more expanded ones