I am currently using R+ Motion 2.0 version 2.3.1 on Windows, along with the OpenCM9.04 controller and XL-320 servos. I noticed that the latest available version is 2.4.17, but I am specifically looking for the installer for version 2.4.11 (Windows).
The reason I am requesting version 2.4.11 is to avoid the “Use maximum speed when XL-320 is synchronized” feature, which was introduced in later versions. This feature overrides our custom speed settings and causes motion issues with our robot configuration.
If anyone from the team or community can share the 2.4.11 installer, I would really appreciate it.
Regarding MOTION V. 2.4.11, you’ll have to wait to see if ROBOTIS folks can help you with that issue.
In the mean time, have you tried to use TASK/MOTION V3 instead?
Also can you share more details about how you use MOTION? Do you just use MOTION directly at run time? i.e. Just use F3 to play the motion units that you created? and always in Sync mode? You can try this option in TASK/MOTION V3 instead too.
What do you mean by “Custom Speed Settings”? Done via “Edit Linked Motion Unit” - like shown below?