ROBOTIS Software
Dynamixel Wizard and the DynamixelSDK for Csharp
Control Environment
Using the XL330-M288-T motors with a U2D2 on a windows device. Testing new features on the wizard and then writing code on Csharp.
Software Description
I am tuning the PID values and i want to save them, the RAM area clears every boot
Issue Description
I am tuning the PID control parameters when the XL330-M288-T is loaded. I get the values and write them to the PID values in the wizard. Is there a way to hard code them rather than writing them at every boot