The DYNAMIXEL Arduino shield hardware isn’t compatible with the DYNAMIXEL Wizard.
You’ll either need to create your own custom arduino sketch to function as a USB to Serial converter, or you’ll need to use A U2D2 or similar device to connect your DYNAMIXELs to your PC.
so i finally go the package and it’s not working though. I am getting the same error.
I’ve used U2D2 3pins to my XL430-W250-T and it won’t scan it. So I’ve clicked the “recovery” but when i unplugged and plugged the cable back into the motor, the progressbar won’t show up neither did the bar fills into 100%.
Now what do I do ? I want to give them ID’s so I can run about 40 motors in the end.