Issue:
I’m using power hub board with u2d2 to connect xl330-m077-t and tried to scan it, but failed. I couldn’t use the firmware recovery tool in dynamixel wizard. Whenever I proceed to the part where it tells me to power off then power on, I followed the instruction but nothing happened. No updating bars appear. I’ve checked the voltage and cable using multimeter, everything is functioning. Weird thing is it happened suddenly because I can scan the motor previously and it runs the code correctly. Same thing happened with my xl430-w250-t motor
DYNAMIXEL Servo:
Couldn’t scan xl430-w520-t and xl330-m077-t
DYNAMIXEL Controller:
power hub board and u2d2
Software Interface:
dynamixel wizard 2.0 latest version 52