Hello forum!
I am trying to control six XL430-W250-T and six 2XL430-W250-T servos, following an example project which uses an OpenCM9.04-C microcontroller to control all 12 servos (or all 18 servos, if you consider the 2XL430’s to be two servos each).
I have very limited experience with servo control, and I am wondering how/if to implement this.
- Would each pair of XL430 and 2XL430 be daisy-chained to each other, so only six connections are made to the controller?
- If each 2XL430 is indeed equivalent to two servos, then can the OpenCM9.04 actually be used, when its capacity is controlling 16 servos?
- Can generic servo controllers be used with generic microcontrollers, provided the servo controllers are capable of handling the power supplied/required?
Thank you!