Hello Robotis, I am using your motor Dynamixel XH series for my project Buliding 3 degree of freedom Robotic arm and it's showing that it used PID controller for controlling but when i Used with U2D2 communication converter with U2D2 power hub then it's c

The PID Controller is built-in/coded inside the firmware for each ROBOTIS Dynamixel - not in the U2D2. For example the ROBOTIS e-manual provides the following information for the XH540-V270 and its PID coefficients when in Position Control mode:

But watch out, the factory default values are usually only set for the P coefficient

Have you seen the following two posts about PID tuning (just on a typical “bare” dynamixel):

2 Likes