Hi everyone
![]()
Though a long-time on my road-map I only very recently got around to extract the custom written C++ wrapper around the Robotis Dynamixel SDK for the L3X-Z hexapod robot into its own C++17 library: libdynamixelplusplus.
One of the major advantages of C++17 from my perspective is automatic type unpacking and incredibly easy iteration over advanced C++ containers (such as std::map or a std::vector of std::tuple). In my humble opinion this allows a almost “functional programming” usage of C++ in terms of achievable code expressiveness.
The code snippet below demonstrates how the library can be used:
#include <cstdlib>
#include <iostream>
#include <dynamixel++/Dynamixel++.h>
using namespace dynamixelplusplus;
static uint16_t const MX28_ControlTable_Torque_Enable = 64;
static uint16_t const MX28_ControlTable_GoalPosition = 116;
int main(int argc, char **argv)
{
Dynamixel dynamixel_ctrl("/dev/serial/by-id/usb-FTDI_USB__-__Serial_Converter_FT4NNZ55-if00-port0",
Dynamixel::Protocol::V2_0,
115200);
Dynamixel::IdVect const id_vect{1,2,3,4};
/* Synchronously enable torque for all servos. */
std::map<Dynamixel::Id, uint8_t> torque_on_data_map;
for (auto id : id_vect) torque_on_data_map[id] = 1;
dynamixel_ctrl.syncWrite(MX28_ControlTable_Torque_Enable, torque_on_data_map);
/* Synchronously set goal position for all servos. */
std::map<Dynamixel::Id, uint32_t> goal_position_data_map;
for (auto id : id_vect) goal_position_data_map[id] = (id - 1) * 1024;
dynamixel_ctrl.syncWrite(MX28_ControlTable_Torque_Enable, goal_position_data_map);
/* Read the current angle from all those servos and print it to std::cout. */
std::map<Dynamixel::Id, uint32_t> position_map;
auto err_read = dynamixel_ctrl.syncRead(MX28_ControlTable_PresentPosition, id_vect, position_map);
if (err_read != Dynamixel::Error::None) {
std::cerr << "'syncRead' failed with error code " << static_cast<int>(err_read) << std::endl;
return EXIT_FAILURE;
}
for (auto [id, position_raw] : position_map)
{
float const position_deg = static_cast<float>(position_raw) * 360.0f / 4096;
std::cout << "Dynamixel MX28 servo #"
<< static_cast<int>(id)
<< ": "
<< position_deg
<< " DEG"
<< std::endl;
}
return EXIT_SUCCESS;
}
Cheers, Alex