Turtlebot3 with Jetson Orin Nano

Dear,

Is there any reference manual for replacing raspberry4 to another board (such as jetson orin mano of NVIDIA)
I am using turtlebot3 which I bought few monthes ogo from Robotis.
So, it would be nice if the manual deals with how to connect/configure the camera, and dynamic cells of turtlebot3.

Best regards,
Se-won.

Regard

I have not used Jetson boards with TurtleBot3 before, but I did use the Jetson Nano with the Engineer kit back in 2021.

And I also checked the Jetson Orin Nano on the Engineer kit also in 2023

I just prepared my Orin Nano as per their official web site info, then install the DXL SDK as normal, it seemed to work fine on both Jetson Nano boards. Video cameras of course worked much better with Jetson because of GStreamer.

In case you are looking at RPi 5, I did a quick check with it at this 2023 post

I would recommend checking out TurtleBot Lime, ROBOTIS Japan’s custom TB3 model featuring the Jetson.

1 Like